This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMCS1101: Current measuement resolution

Part Number: TMCS1101


Can someone help advice what's the measurement resolution of TMCS1101, for example, to measure a curent in range 2~8A, with12bit ADC, is it possible to get resolution smaller than 5mA. and how to calculation the resolution, thanks in advance.

Best Regards!

  • Allen,

    To map the resolution of a magnetic current sensor to an ADC its a two step process. 

    First, you would map the resolution of the ADC least significant bit, Say for example you are using a 5V supply, that means that in the ideal sense, the LSB of a 12bit ADC would be 5V/2^12 = 1.22mV.

    Second, examining the sensitivity of the TMCS1101A1, this is 50mV/A (th e, so we can find the corresponding amperage by dividing by this number, and 1.222mV/50mV/A = 24.4mA

    So the answer here would be no, the resolution of the system is >5mA. To achieve a mA resolution, you can move to higher bit ADC for the A1 variant, or choose a higher sensitivity for the TMCS1101, provided that you're desired measurement range works with the chosen gain. 

  • Thanks a lot Carolus!