This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843AOPEVM: Need some basic information to start development on AWR1843AOP EVM

Part Number: AWR1843AOPEVM
Other Parts Discussed in Thread: AWR1843BOOST, AWR1843AOP, UNIFLASH, , AWR1843, AWR2944

Hi, I have previously worked on AWR1843BOOST. I flashed  "lab0007_medium_range_radar", made my own application software. The performance was very good. Now I need some basic information to begin working on AWR1843AOP EVM, following are my concerns

1. What are the pre-built labs can AWR1843AOP EVM can support, according to link we cannot flash lab007_medium_range_radar on the mentioned device.

2. I am using Uniflash 7.0.0 , and in the devices section I can't see AWR1843AOPEVM, so how to flash a different firmware on the EVM.

3. Currently the EVM is flashed with out_of_the_box demo, so where to get the source code of this out_of_the_box firmware.

4.  Is there any other GUI except the demo visualizer which can directly connect to the radar running out_of_the_box firmware. A GUI that can give a graphical representation in 2D for better visualization.

Thanks