This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843: External QFLASH Memory access

Part Number: IWR1843
Other Parts Discussed in Thread: AWR1642, AWR1843

Hello!

I see in the Evaluation Board of this device that it uses a QSPI Flash memory because it has no internal flash. My question is. Is the code loaded into the RAM from the external memory once at the beginning or is it loaded when it's needed, so it will load code during execution?

Thanks for the answer!!