Other Parts Discussed in Thread: TMCS1107
Hello,
I need to measure current for my application and for that purpose I chose this current sensor and so was currently testing it. I created a small pcb circuit for my application as follows :
I was testing this circuit but was facing some issues. As per instructions I connected a 0.1 uF capacitor b/w Vss and GND and an LED for just power indication. But in my output at 0 A it is Vcc/2 as expected but when I connect a load then it is not able to measure the current properly. Mostly through my observations it was displaying noise and also the frequency from the output was not 50Hz, frequency measured was in Khz for some reasons.
Where am I going wrong here? Is there some other connection required?
Thanks
Avinash