Other Parts Discussed in Thread: PGA460, TUSS4470
Dear Sir/Madame,
We are going to start a new project that consists a residue detection level by ultrasonic level. The power supply is a battery 3.6-3.7V, so we saw that the IC TDC1000 can be ideal for our project because it is 2.7-5.5V and ultra low power, but we have questions:
- Can this IC measure by air?
- The measurement range is up to 8 ms. Is it in miliseconds o meters? If it is miliseconds, the maximum distance is 1.36 meters (340m/s*0.008s/2)? Our preferred maximum distance is 4-5 meters.
You can give us all the information about the ultrasonic detection.
Thanks you and Best regards,
José Manuel.