Other Parts Discussed in Thread: IWR1642
Hi, I used the profile of srr_config_chirp_design_USRR20 in IWR1642 demo,and I encountered the following problem:
When there is an obstacle with a large RCS between 20 and 30m, the radar will detect a false target at close range .
I think it is because the obstacle's distance exceeds the range of USRR20,so I would like to ask if IWR1642 can support setting the bandwidth range of IF filter.
In order to fully suppress the over range target echo signal?