This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: False object heights information

Part Number: IWR6843ISK

Hello everybody,

I have a IWR6843ISK with the MMWAVEIC-Carrier Card.

My Antenna is mounted about 0.89 meters above the ground and I have a beverage box in 5 meter distance in front of the antenna.

If I look at the point cloud with RVIZ, I get the information that the box is about 1.5 meters high. In reality it is only 0.4 meters high.

Does somebody know, where these false information do come from or which config-params I have to change so that I get the right information.

Thanks for help.

Best regards