Other Parts Discussed in Thread: MMWAVEICBOOST
Hi all
I am testing the IWR6843ISK demo board using the people counting lab.
I want detect targets in a <boundaryBox -3 5 0.5 30 -1 3>. We modified the ISK_14m config file to increase max distance.
1) I learned if the maxNumTracks > 20, the system becomes unstable and finally stops.
2) I have lot of errors in the output data stream, the TLVs are shorter than expected. This problem increases as the number of acquired points increases.
I read into the "Group tracker parameter tuning guide" that the maxNumTracks can be increased up to 200 depending on available memory, as well as maxNumPoints, how it is possible to increase the memory ?
Thanks in advance
Alessandro Innocenti
-------------------------
This is the configuration file:
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 7 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
lowPower 0 0
profileCfg 0 60.75 30.00 25.00 59.10 131586 0 18 1 96 2950.00 2 1 36
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
chirpCfg 2 2 0 0 0 0 0 4
frameCfg 0 2 96 0 55.00 1 0
dynamicRACfarCfg -1 4 4 2 2 8 12 4 8 5.00 8.00 0.40 1 1
staticRACfarCfg -1 6 2 2 2 8 8 6 4 8.00 15.00 0.30 0 0
dynamicRangeAngleCfg -1 0.75 0.0010 1 0
dynamic2DAngleCfg -1 1.5 0.0300 1 0 1 0.30 0.85 8.00
staticRangeAngleCfg -1 0 8 8
antGeometry0 0 -1 -2 -3 -2 -3 -4 -5 -4 -5 -6 -7
antGeometry1 -1 -1 -1 -1 0 0 0 0 -1 -1 -1 -1
antPhaseRot 1 1 1 1 1 1 1 1 1 1 1 1
fovCfg -1 70.0 10.0
compRangeBiasAndRxChanPhase 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
% modificato per posizione invertita
staticBoundaryBox -2 4 2 25 -1 3
boundaryBox -3 5 0.5 30 -1 3
sensorPosition 2 0 15
gatingParam 3 2 2 2 4
stateParam 3 3 6 500 5 6000
allocationParam 20 100 0.05 5 0.5 20
maxAcceleration 0.1 0.1 0.1
trackingCfg 1 2 800 20 46 96 55
presenceBoundaryBox -4 4 0.5 12 0 3
sensorStart