This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: P Cascade Radar : number of captured frames

Part Number: AWR1243
Other Parts Discussed in Thread: MMWCAS-DSP-EVM, TIDEP-01012

Hi, 

I am using the TI AWR1243P Cascade Radar evaluation board (TIDEP-01012) with the TI MMWCAS-DSP-EVM Evaluation module (TIDEP-01017). 

I am using the lua script through mmWaveStudio to capture the data: Cascade_Configuratiobn_MIMO.lua and Cascade_Capture.lua. 

I would like to increase the number of frames captured. 

I can change the num_frames_to_capture variable in the Cascade_Capture.lua but the number of frames I save doesn't correspond. Is it the only variable to change? 

In the Cascade_Configuratiobn_MIMO.lua, there are two variables called nframes_master and nframes_slaves, what do these correspond to? Should they be changed as well and made equal to num_frames_to_capture? 

Thank you very much!

Best regards, 

Alice