I want to measure the temperature of the air, but there is something wrong with the assembly. The data found is shown in the following figure. However, I would like to ask how to measure the air temperature outside the shell in a shell? Thanks!
  
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to measure the temperature of the air, but there is something wrong with the assembly. The data found is shown in the following figure. However, I would like to ask how to measure the air temperature outside the shell in a shell? Thanks!
  
Hi Rhea,
The TMP75 in the SOIC8 package can be used to measure ambient temperature, just keep in mind that most of the heat transfer will happen through the leads of the device, as shown in the diagram above. The mold compound (which I think you are referring to as the shell) provides an additional thermal path, but due to its low thermal conductivity, any heat transfer through the mold compound itself is slower than the heat transfer through the leads.
For additional guidance on measuring ambient temperature, please see:
Best regards,
Jesse