Other Parts Discussed in Thread: TMAG5170
Hi team,
Using a magnetic ring with an inner diameter of 18, an outer diameter of 24, a thickness of 3 mm, a total of 6 linear hols are placed in a circle directly below the magnetic ring, with the hall print facing the bottom of the magnetic ring. The circle and the magnetic ring of the Hall distribution are concentric circles with two adjacent Hall spaced 60° apart.
Issue: In this case, the data is not read well and the maximum and minimum deviations are not significant. So the customer would like to know how to determine the position of the Hall relative magnetic ring when designing? And how to get the better data to the Hall?
Could you help check this case? Thanks.
Best Regards,
Cherry