Part Number: AWR1843
Other Parts Discussed in Thread: AWR1443BOOST
Hi, I'd like to ask you a few questions. If I have 2 radars: AWR1843. I would like them to be placed in different locations to detect the same moving target and achieve a bistatic radar (one radar only emits signals, the other radar only receives signals). I noticed this article: AWR1443BOOST: Realization of SPI control using two AWR1443BOOST - Sensors forum - Sensors - TI E2E support forums
1. If I want to implement only one computer to receive data, should I have the same setup for AWR1843?
2. I did not write the source code based on MSS before, just used the software interface to set parameters, how to quickly achieve such a configuration to achieve a radar transmitting another radar receiving this situation?
3. Can you provide detailed steps?
4. After this setting, should I adjust the parameters or check the parameters through the GUI interface on the computer?
5.What affect phase difference and how to achieve phase synchronization?
Thank you very much
Please answer my question! Thank you very much