This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: Reference or demo code for converting captured adc_data_Raw_0.bin to adc_data.bin

Part Number: AWR1642BOOST
Other Parts Discussed in Thread: IWR1642

Hi, 

I am using IWR1642 and DCA1000 for capturing raw ADC data for posting processing. 

With the help of mmwave studio, after configurations, I can get raw data file adc_data_Raw_0.bin, then after click PostProc button, mmwave studio converted adc_data_Raw_0.bin to adc_data.bin.

I am wonder if any reference or demo code for this conversion?

(1) From my observations, both files have the same size which are exact same as the size of captured frames. 

(2) From the tutorial, it said adc_data_Raw_0.bin includes some header information, like Sequence number (4 bytes), Data length field (4 bytes), etc.

If so, how did mmwave studio converted adc_data_Raw_0.bin to adc_data.bin? Any reference?

Thank you so much!

Best,

Hang