This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: Recommended minimum frame period

Part Number: IWR6843
Other Parts Discussed in Thread: AWR1843, AWR6843

Hi 

I am using Interference detection and mitigation lab and have migrated the AWR1843 victim code to IWR6843. I am trying to reduce the frame period as minimum as possible and have disabled all the processing on DSP except the interference detection code in "DPU_RangeProcHWA_process" function. I am able to reduce the frame period till 7.8ms with active frame time around 1.5ms, if I try to reduce less than 7.8ms I am getting an error in the runtime as mentioned below:

Starting Sensor (issuing MMWave_start)
{module#9}: "src/dpm_pipe.c", line 274: error {id:0x10000, args:[0x18b4c, 0x18b4c]}
xdc.runtime.Error.raise: terminating execution

1.Could you please tell the reason for getting the above mentioned error?

2.What is the minimum recommended frame period that can used? 

Thank you

Sachidananda