This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: Frame periodicity in people counting demo

Part Number: IWR6843ISK

Hello everyone,

Increasing the frame periodicity from 55ms will reduce the frame rate? Does changing the frame periodicity to 80 ms affect the demo working?

Thanks and regards,

Aleena N A

  • Hi

    Increasing the frame periodicity allows more processing time for arm to do extra algorithm and decrease RF energy consumption. but also lead to poorer performance. 

    The tracker still works fine if the periodicity is set as 80ms. 

    you may need to adjust some tracker parameters based on the working scenario.