Hello there,
I am going to develop a thermal conductivity gas sensor application like below image.
I don’t yet know a actual bridge output value, but I expect that bridge output value is approximately 0~200mv and it is dependent on tolerance and Temperature Coefficient of sensor heater.
Also, analog output of gas sensor application is 0.5~4.5V corresponding to gas concentration and output resolution is under 0.1V.
I have questions about sensor signal processing.
First, How do I design AFE Circuits using TI’ ICs or others after wheatstone bridge output?
Second, how many bit ADC resolution does mcu need?
I would like to need your many help and ideas.