Hello,
I have two quick questions on using Studio CLI
(1) In order to use the Studio CLI, I guess I need to flash some images. For example, for xwr1642, I flashed mmwave_Studio_cli_xwr16xx.bin. However, for awr2944EVM which tiimage and appimage I should use for raw data capturing? In mmWave MCUPLUS SDK User Guide (4.2.0) page 37, it did not explicitly say it.
(2) For the user's guide, awr2944EVM uses 2 lanes for capturing raw ADC data. Since it is 4 TX and 4 RX, any sample code for parsing the captured (real) data?
Thank you very much!
Best,
Hang