Part Number: LM35
Other Parts Discussed in Thread: LMT70, , TMP117
Hi,
I need to compare the exact uncertainty of LM35 and LMT70.
From the datasheet, We already know the Nonlinearity of LM35CA is ±0.15℃, but this is the case just in -40℃ to +125℃.
Tell me the Nonlinearity in narrower range like -20℃ to 60℃.
Moreover, I want to check this "the output-voltage-versus-temperture curve" that defines Non-linearity.
![]()
↑ is the note in LM35 datasheet.
If you have V-T table of LM35 like LMT70 have, it will help me.
Please show me that.
Best Regards,