Other Parts Discussed in Thread: IWR6843, , UNIFLASH
Hi there,
We are using IWR6843 in a project with the 3dpeople_counting demo. The measurement data is transferred via F14 pin of the chip and to a local pc's COM port through a cp2105. We modified the Baudrate of the demo to 115200 so that the MCU we want to apply for data processing can handle the speed. After some tests on the pc, we are sure the baudrate is appropriate and the data can be recieved by the COM port of the pc without problem. However, when we switch to the MCU and connect the same pin F14 to its Uart pin, no data can be recieved by the MCU. At the moment, we cannot figure out what the problem is. Have we missed something. Could you give some tips?
thx
Shen