Other Parts Discussed in Thread: IWR6843AOPEVM
I.I've been working with an IWR6843AOPEVM. It is reasonably suited to about 75% of my application. For the remaining 25%, I'm detecting objects that are lower on the Intensity signature than the noise floor. Is there a ranking for the TI Radar chips showing the general noise floor for which standard chip and antenna sets?
In other words, I need a chipset that has a lower noise level than what I have now. I.E. I know the object is physically there (in wide open air at a set distance but the radar can't display it because it's below the average noise level.
Thank you,
Peter