This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: The distance between Rx Antenna

Part Number: AWR1843BOOST

When I measured the Rx antenna spacing, it was about 1.85 mm.

This is about the same length as the 81 GHz half wavelength.
Was the length of the Rx antenna designed to be half the wavelength at 81 GHz?