This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: Some questions about the advance frame of 2243

Part Number: AWR2243


Hi all

When  i want to use the advanced frame of this chip, i find that if my bursts is not the same number and the same loop, i can not add different bursts into one subframe.

For example , if i need the first 2chirps is one format and loop 64 times and the next 6 chirps in another format and loop 64 times.

So because the chip just allow us to change the chirp start index but can not change the chirp numbers and loop numbers between different burst

So i have to config this two format into two subframes. and i need make the time between two subframes larger.

Does my words is right? 

Thanks