This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am currently trying to send radar data from an IWR6843ISK plugged onto the MMWAVEICBOOST board to a launchpad plugged onto the boosterpack headers, however I am not able to find out how to do this / which settings (muxing, DIP, etc.) have to be set. The boosterpack header pins J5.5 and J5.6 (RS232 TX and RX) are the only pins which make sense for me, however no data is transmitted according to my oscilloscope.
Could someone maybe point out how to perform this and which UART pins / which UART device has to be used for external UART communication?
Thanks and best regards
Hi Hopfi,
Please see section 2.7.1 in the 60GHz mmWave Sensor EVMs User's Guide. This should answer your questions about connecting the MMWAVEICBOOST to a LaunchPad.
Regards,
Brennan
Hi Brennan,
everything is configured as described in this chapter, however I do not need the whole Launchpad connection but just the UART RX and TX of J5 / J6 . I have just verified everything and still get no signal at all on any of the pins on J5 / J6. Could I have missed some jumper / a specific DIP setting which is need to power the J5 & J6 headers?
Thanks and best regards
Hello,
Please ensure your S1 swtiches are set correctly. To utilize the 40-pin launchPad connectors, the switches must be set as follows:
S1.12 | ON |
S1.11 | OFF |
S1.10 | OFF |
S1.9 | ON |
S1.8 | ON |
S1.7 | OFF |
S1.6 | OFF |
S1.5 | OFF |
S1.4 | ON |
S1.3 | OFF |
S1.2 | ON |
S1.1 | OFF |
Always power cycle your device when changing switch settings.
See Page 11 in the User's Guide for reference.
Regards,
Brennan
Hi,
the S1 switches are set as described in your last post, yet there is no power at all on any of the ports. I just verified this with another ICBoost Board, same result.
Best regards
Hi Hopfi,
Please change S1.5 to ON, and keep the remainder of the switches set as the table shows above. Power cycle and then you should receive power at the ports.
Regards,
Brennan
Hi Brennan,
I have just tried your approach (with a CC26XR2 and also just measuring the ports with an oscilloscope), yet no power seems to be transmitted to those ports. Have you set/changed any other jumpers while trying this out? Currently I a running the following jumper config:
SOP0 bridged
SOP1 open
SOP2 open
J27 2-3 bridged (5V)
J28 2-3 bridged (5V)
J13 fully open
P7 open (5V)
P3 bridged (5V)
J14 1-2 bridged (FTDI/60 pin(J10))
J15 2-3 bridged (XDS110)
S1: as described in your last post + S1.5 ON
Thanks a lot and best regards
Hi,
Your switch and jumper settings seem correct. Can you confirm for me that you have a common ground between the LaunchPad and the ICBOOST? I only ask as when two controllers are 'talking' to each other serially in terms of signals, both micro-controllers should have a common reference point to 'understand' or 'agree upon' what the voltage level of the signal coming from the other micro-controller is. I.e. If one sends 3.3V, the other one needs to read it as 3.3V itself.
Also, if possible, could you post an image of your setup and connections to this thread?
Regards,
Brennan
Hi Brennan,
this is weird. Currently I am not even testing the serial communication yet, I am just measuring the 3V3 and 5V pins (J5, J7, J8) against the corresponding GND pins (J5, J7, J8) on the ICBOOST board (completely without any launchpad) and am still getting 0V on all combinations. The setup thus is just the ICBoostBoard, 5V jack plugged in and multimeter / oscilloscope connected to those different pin combinations. An IWR6843ISK module is also mounted, I have tried to measure the pins with and without the IWR mounted on the ICBoost but without luck. There is also, of course, no LED on when connecting a launchpad to the ICBoost since there is no power. So the problem is that generally all pins on the headers J5-8 are not working, not just the serial ports.
Best regards
Hi Hopfi,
I ran tests on the Rx/Tx pins using a logic analyzer and was able to get Rx/Tx data. I also notice you said you are trying to get data from pins J5.5 and J5.6, however the pin for TX is pin J5.5 and the pin for RX is J5.7.
Is your power supply sufficient? You need at least 5V, 2.5A to power the MMWAVEICBOOST board.
Please also try toggling S1.5 to OFF. It can differ depending on the board rev.
Regards,
Brennan
Hi Brennan,
thanks a lot for your patience and help - I finally got it working with the following config (in case someone needs it in the future):
SOP0 bridged
SOP1 open
SOP2 open
J27 2-3 bridged (5V)
J28 2-3 bridged (5V)
J13 fully open
P7 open (5V)
P3 bridged (5V)
J14 1-2 bridged (FTDI/60 pin(J10))
J15 2-3 bridged (XDS110)
S1.12 ON
S1.11 OFF
S1.10 OFF
S1.9 ON
S1.8 ON
S1.7 OFF
S1.6 OFF
S1.5 OFF
S1.4 ON
S1.3 OFF
S1.2 ON
S1.1 OFF
Thanks and best regards!
Concering the pin layout: there is a difference in the Quickstart User Guide and the EVM User Guide concering the boosterpack pin layout. According to the EVM Guide, J6 6 and 7 are for UART RX and RX (Figure 2-17. TI Standard LaunchPad) and according to the Quickstart Guide it should be J5 5 and 7. Further Figure 2-17. TI Standard LaunchPad and Table 2-4. J6 Connector Pinout dont correspond (J5 and J6 are switched up either in the table or the figure?)
Hopfi,
Thanks for calling that out, I'll see that this is looked into. I'm glad you were able to get your setup working!
The quickstart guide is correct, and the schematics at: https://www.ti.com/lit/zip/swrr164 confirm this.
Closing this thread, if you have any additional questions please open a new thread.
Regards,
Brennan