Other Parts Discussed in Thread: AWR1843
In mmwave sdk, there are debug messages for qspiflash in qspiflash.c as below:
#ifdef QSPIFLASH_DEBUG { uint8_t status = 0; /* Read status */ status = QSPIFlashGetStatus(QSPIHandle, ptrFlashParams->readSR1Cmd); printf("status1 = %x\n", status); status = QSPIFlashGetStatus(QSPIHandle, ptrFlashParams->readSR2Cmd); printf("status2 = %x\n", status); status = QSPIFlashGetStatus(QSPIHandle, ptrFlashParams->readSR3Cmd); printf("status3 = %x\n", status); } /* Debug messages */ printf("--------- SPI flash detected-----------\n"); printf("Device manufacture: %x\n",ptrFlashParams->devID.Manufacture); printf("Device type: %x\n", ptrFlashParams->devID.device); printf("Device capacity: %x\n", ptrFlashParams->devID.capacity); printf("Number of Address bytes: %d\n", ptrFlashParams->numAddrBytes); printf("Erase command: %x\n", ptrFlashParams->sectorEraseCmd); printf("Dual read command: %x\n", ptrFlashParams->dualReadCmd); printf("Quad read command: %x\n", ptrFlashParams->quadReadCmd); printf("Read command support: %x\n", ptrFlashParams->readCmdSupport); printf("------------------------------------\n"); #endif
I add definiton of QSPIFLASH_DEBUG in the file qspiflash.c as
#define QSPIFLASH_DEBUG 1U
I rebuild the qspiflash driver and automotive lab demo: can_sbl (can_sbl uses modified qspiflash driver). From port "XDS110 Class Application/User UART", I can see demo's debug log, but I cannot see driver's debug log.
How can I check qspiflash driver's debug messages?
Thanks