This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR6843AOP: Peripherals in low power operation (MSS clock to 40MHz)

Part Number: AWR6843AOP
Other Parts Discussed in Thread: AWR6843

Champs,

Here is question of peripherals of AWR6843(AOP) when running in low power idle mode.

From "Low Power Demo" of Industrial Toolbox, MSS can be clock down using xWR6843_mss_vclk_40M() function.

When MSS running at 40MHz clock, how to use peripherals of CAN, SPI, I2C, UART, QSP, and QSPI Flash?

From the user's guide of Low Power Demo, "CAN_FD and QSPI" can run on slower clock speed.

   [Q1] So, how about (classic) CAN and QSPI Flash?

   [Q2] If it is possible to use CAN, how to make it working? Is it required to change the configurations every time according to the MSS frequency of 40MHz and 200MHz?

Best regards,

Hayden