Hello,
can you possibly advise on a customer questions regarding the best sensor to use for their following project?
-----
For our project we want to be able to track movements of persons in the outdoor environment.
We want to know which direction they are moving towards and the distance to the sensor.
For our project we want to measure movements from a short and long distance. For example detect movement
from a distance of 1 meter and also 10 meters.
It is important that we can also pinpoint one person to focus on, because we want an object to interact with
the movements of one or two persons. We were thinking about using a mmWave sensor for this.
Is there a type of mmWave sensor you can recommend., or different type in case this could be better suited for this application?
-----
Thank you very much.
Best regards
Adnan