Other Parts Discussed in Thread: MMWAVEICBOOST, , DCA1000EVM
Hello
I have the setup of a DCA1000evm, an mmwaveICBOOST and an IWR6843ISK. It has had a lot of issues, but today, a new one appeared.
Yesterday it worked somewhat fine, once I got around the Calling_ConnectTarget returned 3 error at step 3 in mmwave studio.
But today, there is trouble from the beginning. As step one after opening mmwave studio, I press SetUp DCA1000 and once I press Connect, Reset and Configure, I get invalid lvdsMode value [error -4016].
If I continue from here, I can do reset control, but when I press connect in RS232 Operations, I then get unable to read FPGA version [error -5].
Yesterday, none of those errors came up, but today, it happens consistently. I've rebooted the laptop and reconnected all the wires several times. Nothing helps.
The setup does not work on the other computer I have either, but there, I get no errors before the Calling_ConnectTarget returned 3 error at step 3 in mmwave studio.
I have checked the debug manual, but the only suggestion I see there is about arming and about selecting the right device. I have selected the right device and I don't even get to the arming point before the error message, so it doesn't solve the problem.
It should also be noted that the lamp on my ICBoost board for IWR HW error is glowing red, so maybe my board is just broken, but it is strange how inconsistent it is in whether it will work or not.
The setup worked yesterday or displayed an entirely different error, the one I described in
https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1067739/iwr6843isk-inconsistent-error-connection-failed-calling_connecttarget-returned-3/3960986#3960986
Speaking of which, I am somewhat annoyed that despite my added information on that subject, no response has been forthcoming for several days.