Hi team,
In AWR2243 4x cascade radar HW design, we are using 2 2-way Wilkinson divider to got the 4 20G LO.
But the Wilkinson divider request the 100Ohms resistance, so it must to make the LO trace goes up to TOP layer again through the vias.
Question, customer is asking how to use other types power divider without the resistance, then they can keep the power divider circuit in L3, then it will be less loss in the via structure.
So, their purpose is the LO trace from SYNCOUT BGA pin then goes to L3 directly, power divider is happen in L3, then goes up to TOP layer again and feed to SYNCIN.
Can you please let me know what's the reason to use the Wilkinson divider here? And what's the details spec requirements on this power divider like the insert loss, S11,S12,S23...
Thanks.
Regards,
Wesley