This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP100-EP: What is ESD rating of TMP100-EP?

Part Number: TMP100-EP


Hi Experts

The datasheet for TMP100-EP does not list any ESD ratings.

Can someone provide those please?

Thank you!

Jim B

  • Dear Jim - 

    Thanks for the post. 

    Here, as this is EP product, it has on the product page an Enhanced Product Qualification and Reliability Report. https://www.ti.com/lit/pdf/sglk076 

    and where it lists ESD levels tested to 1kV for CDM and 4kV for HBM: 

    BR-

    Josh 

  • Thanks Josh

    That is helpful.

    Please note that I also checked the link for the material and reliability information. In there it only refers to the datasheet, not the EP Qual report.

    https://www.ti.com/quality-reliability-packaging-download/report?opn=TMP100MDBVREP 

    Qualification summary

    Stress Reference Min lot qty SS / lot Condition Duration Result
    HTOL JESD22-A108 3 77 Life test, 125C 1000 hours Pass
    HTSL JESD22-A103 3 25 High temp storage bake 150C 1000 hours Pass
    AC/UHAST JESD22-A102/JESD22-A118 3 25 Autoclave 121C or unbiased HAST 130C / 85% RH 96 hours Pass
    THB/HAST JESD22-A101/JESD22-A110 3 25 THB 85C/85%RH or HAST 130C/110C/85%RH 1000 hours or 96 hours Pass
    TC JESD22-A104 3 25 Temperature cycle -65/150C 500 cycles Pass
    SD J-STD-002 3 22 Per specification >95% lead coverage Pass
    HBM JS-001 1 3 ESD - HBM Classification See data sheet
    CDM JESD22-C101 1 3 ESD - CDM Classification See data sheet
    LU JESD78 1 3 Latch-up Per JESD78 Pass
    MSL J-STD-020 Per J-STD-020 Classification

    See data sheet

  • Jim - 

    Thanks for pointing that out. The catalog and auto versions of this device do have ESD ratings, it looks like the -EP datasheet needs to be updated from an older TI format, which would by default then have the ESD ratings table that you/we all expected. Again, thanks for your observation.