This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: The relation between the bandwidth and Maximum IF bandwidth

Part Number: AWR2944

Hi

     In the radar waveform design, are the  bandwidth  B and the Maximum IF bandwidth IFmax  equal? Or  are they actually the same?

    When we design the waveform, firstly the ADC sampling frequency is an factor to deside the Maximum IF bandwidth, actually once the Maximum IF bandwidth  is selected, the bandwidth  B can be decided.In the datasheet,the max bandwith can be 4G,but maximum ADC sampling frequency in theTI’s radar devices is 45 MHz (AWR22xx) ,how can the bandwidth 4GHz be  achieved? I am very confused about that .

Thanks,

BR

Rata