Device: AWR2243P ES1.1
Firmware: 2.2.3.1 (xwr22xx_metaImage.bin)
mmWaveLink: 2.2.3.1
Control I/F: I2C
------------------------------
Now we are developing a mm-wave radar module using AWR2243P.
We are trying to control it by using I2C, but it is not working well.
In the radar message sequence, after sending a command from the host,
the AWR generates an interrupt, but the interrupt is cleared before the CYNS takes effect.
Is this behavior normal?
Our understanding is that the interrupt is cleared after CYNS is issued.