I am trying to reduce the power consumption of the device. Right now I am using the IWR6843AOPEVM with the break away section removed. I have it configured to have a chirp duration of 28us, using all 3 TX antennas, with 32 loops, and a burst period of 25ms. By my math this means I should be running at about 10.8% duty cycle ( 3*32*0.028/25 = 0.108). Based on this chart from the data sheet I should be seeing a power draw of around 1 watt for the device. However, when I measure the power draw of the radar I typically get 2.1 watts before I start the sensor and then 2.41 when the sensor is active. Is this typical of what the sensor should be drawing and how can I reduce the power consumption?