Other Parts Discussed in Thread: AWR2243,
Hello,
I was using MMWCAS-RF-EVM (AWR2243) and MMWCAS-DSP-EVM for antenna calibration referring to C:\ti\mmwave_studio_03_00_00_14\docs\mmwave_studio_cascade_user_guide.pdf on page 30.
Everything goes smoothly and the calibrateResults_high.mat can be generated from the captured data with MIMO configuration (with file Cascade_Configuration_MIMO.lua and Cascade_Capture.lua).
However, I got wrong target range estimation when I run cascade_MIMO_antennaCalib.m, "Target is estimated at range 4.7477"


Actually, the target was placed at a distance of 5.2 m to the corner reflector. Below was the setup. As you can see there was no other strong reflector around.


I also tried to set "targetRange = 5.2;" in cascade_MIMO_antennaCalib.m. I still have "Target is estimated at range 4.7477".
Since I got wrong target (corner reflector) range estimation, the generated calibrateResults_high.mat might not be valid.
My question is that what was the possible reason I go this wrong target estimation? Or what I should do to fix it?
Thank you very much for the help!
Best,
Hang