Other Parts Discussed in Thread: IWR1443, TIDEP-0091
I have an MSP432 and an IWR1443 and I am trying to connect them using the level sensing reference design. The only issue I am having is that the sdk 2.1 which this design calls for also requires the IWR1443 to be an ES3.0. I however only have access to an ES2.0. To buy a new 1443 would cost around $350 which, unfortunately, is out of my budget. Is it possible to get these two devices to communicate? Could I change the .bin file to allow it to flash the ES2.0 correctly? I'm sure someone has done it before. Any help would be greatly appreciated.