Hi all,
I would like to implement 'listen before talk', scanning the spectrum before starting the actual radar waveform.
To do that, I need to generate chirps with the transmitter turned off. The receiver would be working normally and receiver LO would still be chirping, turning the AWR18 into a swept receiver that catches transmission from potential interferers.
I am using the mmwave SDK 3.5 AWR1843 OOB demo:
The only option to chirp with little Tx output appears to be setting the Tx power backoff to its maximum of 20 dB. Ideally it would like to reduce the transmit power further. Disabling the Tx in the "channelCfg" or "chirpCfg" CLI commands leads to an error.
Is there a better way to achieve the desired behavior?
Best regards
Sebastian