Part Number: TMP121
Other Parts Discussed in Thread: TMP123, TMP125
Hello,
Got a fairly straightforward question regarding the TMP121/TMP123 and was looking to see if someone could help clarify something regarding the SPI output.
What is the SPI SO pin output from these devices if the CS pin is continuously held low? Will it continuously clock out the 16-bits containing the temp data from the most recent conversion (for example, the same as the TMP125) or will it only clock out the data once and then go into an idle/shutdown state until CS is released and re-asserted low?
Thanks,