Hi Champs.
There're several questions about IWR6843's Antenna below.
Please help us to get clarified.
- Antenna Performance Specification for Tx & Rx of IWR6843 device.
- Range of deviation that allows the difference in three Rx's perforamnces.
e.g. Performance deviation is within 1dB btw Rx1, Rx2 and Rx3.
- Custom design would apply the Antenna with 1x Tx and 3x Rx. Is it applicable with IWR6843 since it has 3x Rx and 4x Tx. How to handle 3 extra Tx?
- Is it possible to connect DWFC type Antenna to 6843 EVM Kit?
- Is it possile to adjust the respective Antenna Power?
- How to measure the Antenna performance of 6843AOP type?
- Does each Antenna have a mobile switch?
Thanks.
Regards,
Jack