This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP464: Short circuit detected for application not using one chnnel

Part Number: TMP464


Hi TI team

We are using TMP464 in an application where D1 is not used and hence connected to D- as indicated in the datasheet

the strange thing is that with this configuration, we detect a short circuit to GND on both these pins: this means D1+, D- and D are in short when probing with a multimeter

On the other side, the component is working fine on D2, D3 and D4 channels, where temperature reading is correct

is the D- pin internally connected to a "clean" ground reference even if this is not shown on the block diagram?

any reason that could explain this issue?

thanks in advance

Alberto