This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: The syscfg of the timer in the MSS demo

Part Number: AWR2944

Hi,

   I want to configure the period of the timer  as 10ms, my configuration is as belows:

  

  In this configuration, the period is still 1ms,if I configurate like this

The configuration will work,and the period of the timer will change to 10ms.That  is to say. If I want to set the period as 10ms, the two points must be modified and should be consistent, is that right?

  I notice that the tick perod scopes are different, in the CONFIG_TIMER0, the scope is 1.0 to 1000000.0,but in the Clock, it is 100.0 to 1000000.0.Why are they different?

BR

Rata