This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: Sense and direct HVAC control not working

Part Number: IWR6843ISK
Other Parts Discussed in Thread: MMWAVEICBOOST

Hello everyone,

We have a requirement that uses the lab sense and direct HVAC control. The EVM was flashed with the bin file of the same. We are using it along with MMWAVEICBOOST. After flashing it was set to functional mode but the yellow LED at top(DS2) is still ON, it is not turning OFF in functional mode(when people counting or long-range bin files are flashed and put in functional mode the LED DS2 will be OFF). Is it like that?

Anyways we ran the mmwave people counting GUI and selected Sense and direct HVAC control from the drop-down and selected the corresponding cfg. But nothing was detected. Some points are shown but no tracks were shown. Frame number was increasing. How to resolve that?

Thanks and regards,

Aleena N A