Sir,
As the following profile, TX no backoff & RX gain is 40dB or 30dB?
profileCfg 0 77 3 3 24 0 0 15 1 256 12500 0 1 40
if I want to backoff 10dB for all of TX1, TX2, TX3, may I know if I need to modify this profile as
profileCfg 0 77 3 3 24 657930 0 15 1 256 12500 0 1 40
Moreover, if I want to further reduce the total RX gain into 26dB, if I need to modify as
profileCfg 0 77 3 3 24 657930 0 15 1 256 12500 0 1 216
which is RX gain as 26dB, RX VGA gain as 24dB
JY