Part Number: FDC1004QEVM
Other Parts Discussed in Thread: FDC1004, TIDA-00317, , FDC1004EVM
I am attempting to use the FDC1004 to do liquid level detection, following the design reference document: Capacitive-Based Liquid Level Sensing Sensor Reference Design . Using the FDC1004QEVM and a flex cable based on the TIDA-00317 reference documents, I am having issues getting the expected results.
Below is a picture of my setup:
Using the Sensing Solutions EVM GUI, here are the configurations:

By filling up water to the relevant cm, I am getting the following results:
| 2 | 3 | 4 | 5 | 6 | 7 | 8 | 7 | 6 | 5 | 4 | 3 | |
| Clevel | 2.06 | 2.17 | 2.23 | 2.3 | 2.455 | 2.68 | 2.815 | 2.789 | 2.76 | 2.736 | 2.675 | 2.07 |
| RefLiquid | -0.841 | -0.842 | -0.846 | -0.854 | -0.851 | -0.85 | -0.85 | -0.85 | -0.85 | -0.85 | -0.85 | -0.82 |
| refEnv | 4.755 | 4.756 | 4.75 | 4.76 | 4.76 | 4.77 | 4.78 | 4.77 | 4.76 | 4.76 | 4.75 | 4.75 |
I am not seeing the changes in capacitance I expect from the Clevel and refLiquid measurements. Even with the small, consistent deltas when adding water to the container, while removing liquid, the values do not return to a consistent measurement. I've attempted with a couple different containers but the results are similar to what's described above. Is there something incorrect in my setup (physically or materially)? Do I have something configured incorrectly in the settings?
Any insight would be greatly appreciated!
Thanks