This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: two AWR2243 cascad

Part Number: AWR2243

Our company adopts two AWR2243 cascade schemes, 20GHz LO connection is as follows: Master AWR 2243 FM_SYNCOUT  connects to 2-way Splitter to feed Master AWR 2243 FM_CW_SYNCIN1 and Slave AWR 2243 FM_CW_SYNCIN1(Note:2-way Splitter and PCB stackup  refer to TI  4-AWR 2243 cascde demo,Program code refers to newest dfp)。 During debug, some phenomenon are founded:

(1)、Sweep frequeny within the scope of 76 ~ 77 GHZ,LVDS output of Master AWR2243  is OK,LVDS output of Slave AWR2243  is about 0。Sweep frequeny within the scope of 77 ~ 81GHZ,LVDS output of Master and  Slave are about 0。

(2)、If two AWR2243  are set to single-chip mode,Sweep frequeny within the scope of 76 ~ 81 GHz,LVDS output of two AWR2243 are OK。

Please ask:20GHz LO connection is OK? Program code need to modify?