Hi Shankar:
Please consider this a continuation of the locked forum thread linked below due to my being "redirected" for some time (sorry about that)...
Before we continue, I was told some time back that the only problem we might have using the system without the IQMM calibration is that we wouldn't be able to do noise detection. We did not consider this to be a problem because we do not intend to do noise detection.
However, I'd also like to know if the lack of IQMM calibration could cause the amount of baseline noise to differ between systems that are identically configured. We have noticed that some of the systems exhibit differing amounts of baseline noise even though they are being operated at the same gain settings. Could this be caused by the lack of IQMM calibration?
Thanks, Michael