Hi,
Does the AWR2243 have a port that can be used to test the sensitivity of the RX received signal?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Does the AWR2243 have a port that can be used to test the sensitivity of the RX received signal?
The customer wants to do the following test. After the signal received by the RX is processed by the internal low-pass filtering of the chip, the signal before the ADC is compared with the input signal.
Some manufacturers' chips will have special pins for this function test. I want to confirm whether the AWR2243 supports this function?
If it is not supported, have you conducted similar tests internally, and have you reported any reports?
Hello Nancy,
I am not sure I understand the request fully. If we feed a 1Mhz offset tone (RF frequency + 1 Mhz) at the RX LNA input we can get a 1Mhz tone in the ADC data. Is that what you are suggesting?
Regards,
Vivek