This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: Hi,I am using AWR2243 Cascade Radar EVM and TDA2xx, I have some questions about the number of ADC sampling points

Part Number: AWR2243
Other Parts Discussed in Thread: TDA2

Can I be in Process_ SDK_ RADAR_03_ 08_ 00_ 00 set the ADC sampling points of awr2243 to 1x complex sampling of 1024? but in the document "mmwave studio cascade user's Guide.pdf" “The maximum number of samples per chirp is currently limited to 512 in complex 1x/2x modes, and 1024 in real mode. This is a limitation of the TDA2. There is no workaround at this time.”