This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA970: Debugger connecting erroe

Part Number: PGA970

Hi ,

        After working with PGA970, developed PCB for PGA970 finally board tested for programming using XDS200 BALCKHAWK debugger

         but while connecting getting error

  " Error connecting to the target:
(Error -615 @ 0x0)
The target failed to see a correctly formatted SWD header. The
connection to the target may be unreliable. Try lowering the
TCLK setting before trying again.
(Emulation package 9.5.0.00143)"

     need help in this ,tried checking several time the connection is ok but  still error in this. 

Thanks & Regards,

XAVIER

  • Hello Xavier,

    Please make sure you have set up the target configuration file as described in the Software Quickstart Guide. You should be able to run the Test Connection routine and get a success message from the target configuration settings box in CCS.

    Regards,

    Scott

  • Hi Scott,

               Yes followed the steps provided in datasheet you mentioned ,when test connection given the following results given, but problem still not solved.


    [Result]


    -----[Print the board config pathname(s)]------------------------------------

    C:\Users\ADMINI~1\AppData\Local\TEXASI~1\
    CCS\ccs1100\0\0\BrdDat\testBoard.dat

    -----[Print the reset-command software log-file]-----------------------------

    This utility has selected a 560/2xx-class product.
    This utility will load the program 'xds2xxu.out'.
    The library package version is '9.5.0.00143'.
    The library component version is '35.35.0.0'.
    The controller does not use a programmable FPGA.
    The controller has a version number of '13' (0x0000000d).
    The controller has an insertion length of '0' (0x00000000).
    This utility will attempt to reset the controller to enter SWD mode.

    -----[Print the reset-command hardware log-file]-----------------------------

    This emulator does not create a reset log-file.

    -----[Perform the SWD Mode Integrity test]-----------------------------------

    This test will read the IDCODE register 1 time.

    The IDCODE register value is 0x0bb11477.

    The SWD Mode Integrity test has succeeded.

    [End: Texas Instruments XDS2xx USB Debug Probe_0]

    Regards,

    Xavier