The following question is related to:
C:\ti\mmwave_dfp_02_02_03_01\ti\example\mmWaveLink_Cascade_Example
When running an Advanced Chirp / Advanced Frame test, the captured data file(s) are smaller by the exactly the size of one subframe.
All 4 files (master_0000_data, slave1_0000_data, slave2, slave3) are exactly the same size and all are short 1 sub-frame bytes
parameter settings are:
IDLE TIME = 2uS,
RAMP_END_TIME = 23US,
(Chirp cycle time = 25us)
#TOTAL CHIRPS = 12
#BURSTS = 5
BURST PERIOD = (25us *12) + 110us + 25us extra
OUTER_LOOPS = 2
#SUBRAMES = 4
SUBFRFAME PERIOD = (#BURSTS * OUTER_LOOPS) * BURST_PERIOD + 345uS + 400us extra
#FRAMES 1 to 20
If I run 1 FRAME, the capture files are the size of 3 Subframes (not 4), with one missing
If I run 20 FRAMEs, the capture files are the size of 79 Subframes (not 80), with one missing
I don't know which SF (first, last, other) was dropped from the capture files
Any ideas what could be causing this:?
Regards
Eddie