Other Parts Discussed in Thread: DRV5056, DRV5057, DRV5053
Hello,
We currently use the DRV5055A3QDBZR in our design. Unfortunately, global supplies are zero. It appears that Mouser has some DRV5055Z3QDBZR.
1. From the data sheet, it appears the only difference between the two is that there is temperature drift compensation on the A3 and not on the D3?
2. As I understand it the drift is .12%/degree celcius. So, if our device is tuned at 25 degrees Celcius andbused in a temperature range of 0-50 degrees celcius, there is a +/- 3% (+/- 25x.12) drift for the Z3.Is this correct?
3. Are there any other direct substitutes for the DRV5055A3QDBZR that you can recommend?