Hi.
I am evaluating the IWR6843AOPEVM module and I have successfully run the Area Scanner demo lab (4.1.0) with the default configuration parameters. After that, I tried to increase the detection range of the dynamic objects to 30m. I have tuned the profile parameters using the OOB demo and successfully detected large objects at 30m. I copied the new parameters into the Area Scanner config file and gave it a try. However, the dynamic point clouds are still limited to 10-11m.
I have tried multiple parameters yet the max range still never gets past 11m. I am not sure if I have misconfigured something. Here is my current profile parameters in the config file compared to the default file.
-New:
-----------------------